Other Parts Discussed in Thread: TPS2121
Hi,
Is the TPS2113A allowed to have a voltage applied to the OUT pin without a voltage on the IN1/IN2 pins (\EN tied to GND)?
In my design it is possible for a user to swap two connectors. In that situation there will be a maximum of 5,3V applied to the OUT pin (indefinitely). The IN1/IN2 pins will be at 0V. I assume this won't be a problem because a large capacitance on OUT will place it in the same situation if the inputs are powered down (albeit for a short period).
Regards,
Robbert