Hi, TI team.
My customer will design battery charger for 2600mA battery.
BQ24073 can set current limit by 1.5A.
Test condition
DC power supply : 5V, 500mA
BQ24073EVM : charging current 1A. (external setting)
Result : DC power supply voltage dropped to 4.4V.
When the charging current limit of BQ24073 is set to 1A, If user will use 500mA DC adapter, Is DC adapter possible to be damaged?