Please let me confirm about way to measure OVP function for TPS53015.
I think that the method of measure OVP function is below, is it correct?
①Low side feedback resister set to short (for example, R2 resister by datasheet Figure18)
②Confirm to measure increasing Vout and occur OVP function on Vout ×120%
【Background】
・Vin: 12V, Vout: 5V, Iout: 4A
・When measure above method, OVP occurred on 8.2V, not 6V.
I guess that effect of OVP propagation delay (10μs), is there any other reason?
※X-axis: 200μs/div, Y-axis: 5V/div
Best regards,
Satoshi