Other Parts Discussed in Thread: BQ24232HA, , BQ24079, BQ24072, BQ24073, BQ24230
HI
The customer wants to end the charge at 45 when using the bq24232HA.
I learned about BQ24079T during the search as below.
However, it is difficult to apply because the input voltage is 6.4V.
Is there a product with higher input voltage that uses voltage-based TS bias like BQ24079T?
"The bq24079 (T) ICs are regulated to 4.1 V. The "T" version uses a voltage-based TS bias, which allows more flexibility in setting the temperature range, while the bq24072 / 3/4 / .
The bq24230 / 2 family is identical to the bq24073 / 4 ICs except that they are trimmed and their targetcurrent values are nominally at 300mA (<450mA). This family is suited for headset designs. The pinout of each IC is the same across both families except pin 15 (JMP2 on the EVM); The pin 15 function is listed in Table 1 under the Optional Function column."