Other Parts Discussed in Thread: BQ25504
I have bq25504 evaluation board which energy harvests from indoor light using a small solar panel. I am going to feed the harvested energy to a smoke alarm at 10V to replace the usual 9V alkaline battery used in such smoke alarms. My bq25504 evaluation board outputs 3.2V nominal and I am looking at the TPS61096A device to step the voltage up to 10V. The device doing the step-up must be "as low energy consumption as possible". I do not plan to use the shutdown feature of the TPS61096A - the load should never be disconnected by definition for a smoke alarm. SO!, MY QUESTION: What is typical current consumption of TPS61096A during normal operation when it will be supplying a maximum of 10uA to the smoke alarm for all time ?
Best Regards, John O'Connor