This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We refer to the soft-star schematic of LM2611 datasheet in our design, and the voltage is step up from 12V to 12.8V(input 12V and output 12.8V),
the PCB is short circuit when the power on, can you help to check the schematic and give us your suggestion, thanks?
The schematic for your referenc
Hi Brigitte,
Very thanks for your quickly reply.
The below is the answer of your questions:
First, there is no problem which we measured output voltage is -12.8V, R222 is 100K and R223 is 11K, we would like to know the output voltage(-12.8V) reasonable or not?
We can not find the reference in the datasheet.
Second, I have changed capacitance of C287 to 1UF, there is no help.
Third, I use fxc0630-220m /22UH/ 4A which integrated forming large current patch power inductor and the dimensions are 7*7*3mm.
Fourth, The circuit is short out when power turn on, nothing to do for the PCB.
Fifth, it is no help to remove R220, I have disconnected and tried with no-load.
The inductance as below picture:
Hello user5973782,
I am sorry, but I am a bit confused about the issue you have.
1. -12.8V seems to be ok, because if I calculate with the given -1.23V feedback voltage and your resistors, I get to -12.4V. The difference in voltage is possibly caused by the resistor divider. It is mentioned in the datasheet that it is recommended to use values below 50 kOhm.
2. You mention that there is a short when you turn on the power supply. What exactly does this mean. Is there more current on the input than you expect? How many boards do you have that show the problem?
Does it change the behavior of the circuit when you remove the startup capacitor connected from /SHDN to VOUT?
Hello user5973782,
Therefore I will close this discussion for the moment. If you have more information, either post again in this thread or start a new one if this one is locked.