Dear Sir/Ms.
Refer datasheet 9.2.1.
What is the difference between using VBAT2 and VBAT1 input?
As described on the reference circuit, is the Full Bright when the power supply is connected to VBAT2, and the current is controlled by adjusting RADJ1?
Is it Low Bright when connected to VBAT1, and the current is controlled by adjusting RDIM1?
http://www.ti.com/lit/ds/symlink/tps92692.pdf
Best Regards,
Kami Huang