Other Parts Discussed in Thread: TPS737
Hi ,
Our spec is Vin=5V, Vout=4.75V, Imax=0.4A.
Can TPS73701 meet its spec?
If not, do you have another suggestion?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
Our spec is Vin=5V, Vout=4.75V, Imax=0.4A.
Can TPS73701 meet its spec?
If not, do you have another suggestion?
Hi ,
Yes TPS737 is able to fit your application conditions stated. Dropout is linear with respect to output current as shown in Figure 3.
As such we can use a simple ratio and the dropout specification provided in the Electrical characteristics table.
Vdo_0.4 A / 0.4 A = Vdo_1 A / 1 A
Vdo_0.4 A / 0.4 A = 500 mV / 1 A
Vdo_0.4 A = 200 mV
Since your application has more than 200 mV of headroom (Vin - Vout), TPS737 will be able to achieve a regulated output.
Very Respectfully,
Ryan