Tool/software: WEBENCH® Design Tools
Hello,
we are using LMZ12003TZ-ADJ/NOPB 9.0V-17.0V to 5.00V @ 2.0A as power supply for a single board computer application. We use the schematics and circuit board layout from the Webench (as far as possible). Unfortunately we have some problems:
1. On some 12V power supplies the single board computer does not boot. The LMZ12003 outputs voltage, so that the LEDs of the SBC are turned on and also the backlight LEDs of the display. When using a 12V battery there is no problem.
2. When the input voltage of the LMZ changes quickly, e.g. an other big consumer load is turned on at a battery application, the SBC turns off immediately. After a few seconds the SBC boots again when the same load and voltage level is applied.
Do you have any recommendations how to improve these behaviours?
Thanks and best regards, Stefan