Hi all,
We are bringing the power supply with TPS40060 up and there an issue, that is both the upper and the lower power mosfet SI7415DN and SI7850DP are too hot. We have one board has this mosfet pair burned if not use heatsink and colling fan for them.
these mosfet PN got from reference design from TI with the same 48VDC input, the differences are on reference design, the output voltage/current is +3.3V/5A, in our design, the output voltage and current is +12V/4A.
Appreciated if you Guru could advise us on:
- Is there any way to reduce power lost on these power mosfet? Could we reduce switching frequency to do that? if frequency reduced, which component(s) should be changed along with?
- Is the compensation circuit affect to mosfet power loss (Both switching and conduction losses)?
- Could we reduce the input voltage to reduce the switching loss? in this case, which component(s) should be changed along with?
- In case we must change the mosfet device for next revision, what is the recommendation for our case? Which package is recommended? Current package is PowerP AK SO-8 and PowerPAK 1212-8.
- Is it better in term of reducing power loss on these Mosfet if we step down the input voltage to 24V, then from 24V step it down to +12V?
Thanks and regards
Triet Tran
**************************************************************************
Finally we have re-designed the TPS40060 circuit to resolve the thermal issue. Please let us know if these new MOSFET are OK for this design:
- The lower Power MOSFET: NTB6412ANG from Onsemi - 100V, 58A, 18.2mOhm - D2PAK package
- The upper MOSFET: SUM110P08-11: 80V, 110A, 110mOhm, TO263 package
Please see the attached datasheet for these MOSFET.
Thanks
Triet Tran