Hi sir,
I was trying to design a constant current LED driver circuit with UCC28810D for the LED 90V,1.2A. But not getting theoutput.Can you help me spot the problem areas?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sir,
I was trying to design a constant current LED driver circuit with UCC28810D for the LED 90V,1.2A. But not getting theoutput.Can you help me spot the problem areas?
Hi sir,
Sorry for late reply. I verified the Pin 4 of D17 is connected to primary ground. However there is an issue that VDD pin without connection is 18V. But as soon as the IC is connected the voltage becomes 13V. And the output at the Gdrv pin is not triggering the external Power Mosfet. What is the voltage range that should be in GDRV pin? Current is less than or equal to 750mA(from datasheet). Please help. Thank you in advance.
Regards
Mohitha
Hi sir,
I mean without connecting ic it is 18v ic but once I connect ic voltage drop occurs from 18v to 13v. I changed ic and checked. Same issue persist. Is it because of the circuit between gdrv pin and gate of external mosfet? Is that part necessary or can we connect directly is gdrv to power mosfet.?
0116.Schematic_ucc28810_Sheet-1_20190503174412.pdf
Hi sir,
I checked vsense pin. It was working fine. I modified the circuit as you said but the resistor R11 got burned. It was 2 watts resistor. Another time schottky diode D8 got burned. Why is it happeningg? The circuit at the output given to EAOUT pin has any problems? should i give any protection?can you suggest some protection?Thank you in advance
Hi sir,
Can you help me find the number of turns, currents it support and core area of transformer T1 used in Pmp4862.