Other Parts Discussed in Thread: TPS56637
Hi~
Currently, customer is evaluating TLV62585XDRL and found its transient is not good enough.
His test condition are
1. Input: 5V or 3.3V
2. Output: 1.2V/3A
3. Inductor: 1uH
4.Output cap: 22uF x2
5. Transient from 0A to 3A
This result 80mVp-p and add 22pF will improve to 68mVp-p
And 33pF is around 65mVp-p.
Is there any suggestion for LC and CFF design?