This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62585: OVP / UVP

Part Number: TLV62585

Hi E2E,

Did TLV62585  have no OVP/UVP function?

How does IC to protect VOUT over/under voltage?

Thanks!

  • Hi Julian,

    TLV62585 does not have OVP/UVP function although PG pin indicates the status of the Vout (refer to datasheet for details). In application that requires protection of the system, an external housekeeping IC can be used to monitor the Vout level and has the capability to disable the device in case of fault condition. By the way, OVP and UVP conditions will not cause the device to damage.


    Best regards,
    Excel