This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We are using the TI ISO5451 in an existing gate Driver circuit.
For driving SiC-semiconductors, we would like to add the recommended external current buffer circuit of the datasheet (pic below) to get more peak output current ability.
Is it still possible to use the active miller clamp function of the TI ISO5451 by connecting Pin7 to the gate of the SiC-semiconductor directly?
The clamping becomes active when the gate voltage is below 2V. Could this result in a problem, if the internal clamping device is active without knowing the actual gate voltage at the SiC-semiconductor?
Thank you for your help.
Tobi
Hi Audrey,
Thank you for your reply. You are right, somehow the pic was not included. Now you should see it above.
Good to know, that the miller clamping can still be used. As you wrote, the intention is either to use the miller clamp with a unipolar gate voltage supply, or the pull down BJT and supplying the gate with a bipolar voltage without connecting Pin 7 to the gate.
Please let me know if you agree or something is incorrect.
Thank you and best regards,
Tobi
Hi Audrey,
Thank you for your detailed Feedback that helps a lot.
Best regards,
Tobias