This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I am Alec Chen. FAE form WT. Our costumer have used TPS65094 in their design. And when they are measure the power up sequence which they fellow Intel spec for power on sequence control( please see as below, the S3/S4 signal up at the same time), they fine out that the power on sequence is difference form TPS65094 spec.
Below is the power on sequence that they measure which PV1P8 power up before VDDQ, PVSM power up later than P12V, PVCC5, PVCC3 and PVCCRAM power up earlier than VTT,VCCGI. And they didn't match the power on sequence in TPS65094
And We find the difference between the waveform that measure and TPS65094 spec about the S3/S4 sequence . The Intel spec show S3/S4 signal are high are the at same time and TPS65094 spec show S3 and S4 are not high at the same(please see the power up sequence in the spec) and that is why there are difference power om sequence between those two.
We have explained to RD about this and they still concern about the power on sequence doesn't matching and they need TI's help to confirm the power sequence that they measured which following Intel spec is ok for TI design. Therefore, please kindly help us check the waveform that measure and let us know if that is ok .
Above ,please kindly help us checking this and hope to hear form you soon
Cheers
Alec