Other Parts Discussed in Thread: TPS62097
LMR14206 failures issue
We have a design 24v/12v input to 5 v rail typically 20mA, max 100 mA using a LMR14206.
The 5 V rails feeds a TPS62097 Step Down Converter for the 3.3 V rail. Again typically 20mA, max 100 mA.
Both designs are straight out of the data sheet and Webench tool, and I can send copies of the circuit and layout.
PCB layout is 4 layer PCB with ground plane and the layout around the ICs seem reasonable to me.
We ran a batch of 100 and maybe had one or two issues in this area, but they were not repeatable.
We ran a second batch of 200 and 3 failures out of the first 20 tested! Still investigating but it would seem both ICs fail at the same time with the 3.3V step down input appearing to be short to ground (TBC).
It seems to run for a short time then fail. At least one appeared to occur when we stepped the input up from 12 v to 24 volt. The 24 volt is applied via a fairly standard EMC and spike protection circuit we have used for years, so I feel it is unlikely to be input voltage spikes.
At this time it is not evident what failed first.
Any suggestions welcome