This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I have a question about the ramp up of the PowerGood Signal in the TPS54325.
I designed a power circuit which the power good signal pulls up the VREG5 pin(#3) throught a 10k resistor.
When I measured start up waveform, I confrimed the glitch in the Powergood signal(ch4).
Could you tell me about the cause of the glitch?
Does this problem hardly affect?
Best Regards,
keisuke
Hi,
Please use a 20k - 150k resistor as datasheet recommended and try again. The power-good function is activated after soft start has finished, there might be some external noises on Pgood before start-up.Thanks.
Dear lven
Thank you for your reply.
I remeasured a waveform of Powergood signal after a pull up resistor change to 100kohm.
But the glitch is still appear.
Best Regards,
keisuke
Hi,
It looks like the glitch is coupled by a current path, could you please also probe Vin/Vout current? And what's the value of VREG5 capacitor? If possible, could you please attach its schematic and layout? We will also check the issue on TPS54325EVM, thanks.
Hi Iven
I measured the Vin/Vout current waveform.
Those waveform were normal.
I couldn't find the glitch in current waveforms. I haven't the TPS54325EVM,
so could you please check if the PowerGood signal has the glitch?
Best Regards,
keisuke
Hi,
Could you please attach your components values and what's your input and output voltage/load? Thanks.
Hi Iven
Thank you for your adivce.
I describe some componets values of TPS54325 circuit.
- Vin : 12V
- Vout : 1.2V
- Io : 1A(max)
- Cin : GRM21BR61E226ME44L (22uF/25V) x 3pcs ,
GRM033R6YA104KE14D (100nF/35V) x 1pcs
- Cout : GRM21BR61E226ME44L (22uF/25V) x 2pcs
- L : SPM6530T-1R5M100 ( 1.5uH)
- VREG5 pin : GRM188R61H225KE11D (2.2uF/50V)
Best Regards,
keisuke