This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
from lp5951 datasheet, psi=1.3degC/W for SC70 package and 11degC/W fro SOT23 version.
can you conform psi metric for SC70 is correct ? i would assume it is 13 in place of 1.3.
best regards,
Paul
Hi Paul,
The Thermal Information table metrics for both the SC70 and SOT23 packages of LP5951 are consistent with our thermal models. These metrics are modeled on a JEDEC Hi-K board. The following Application Report provides additional information on these metrics and assumptions made:
Please keep in mind that application specific conditions such as board layout will impact the thermal performance of a linear regulator. The following Application Report details how board layout can impact thermal performance.
http://www.ti.com/lit/an/slvae85/slvae85.pdf
Very Respectfully,
Ryan