This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62736: Resistor Network

Part Number: TPS62736


Team,

I plan to use the 4 resistor network (with VIN_OK pulled to VIN to disable) and need to know how critical the 13MOhm sum is to the operation of the circuit. Being size constrained I want to use 2ea. 0201 resistors for this purpose and 6.xMOhm 1% resistors are very difficult to source. If the series resistors sum to 1MOhm for example, does this adversely impact the operation of the TPS62736?

Thank you.