Other Parts Discussed in Thread: UCD7138, UCC24612, UCC28780,
I need to swim across this vast amount of info regarding LLC converter using UCD31348, LMG3410 & sync rectifier with UCD7138 ..but I am in a storm so to speak.
I have already written a few questions I think we would like to discuss..
But now I notice the eval kit used UCD7138, a 6A driver for EPC2024!
Why would this be needed if the scheme is not different from the application of UCC24612 ? Where a diode drop equivalent is sensed to derive sync timing signals....in that application, of course, a MOSFET is used with power flow in reverse direction ( i.e. source to drain)
We are already using that for another module where we use EPC2024 as well! With the help of EPC app, we figured out how to to use UCC24612 for the sync drive of 5V( you can trace that conversation in the posts)
Seems to me the same can be used here excepting the floating drive power: we can manage that!
Appreciate any help in this matter.