Other Parts Discussed in Thread: PMP, TPS2373-4EVM-758, , , PMP20551
Team,
I am looking for advises (like TI reference design, app notes) for the below scenario:
- POE/POE+ with 16 to 57Vin -> 24VDC / 2A
- POE/POE+ with 16 to 57Vin -> 12.5VDC / 2.5A
-Do we have some TIDA/PMP that can support BUCK and BOOST for PoE with above specs?
-What do we advise for such scenario? The idea would to have a similar controller for both use cases.
-Can the TPS23756EVM or TPS2373-4EVM-758 be used with in conjunction of a DC/DC EVM as a proof of concept for the above specs?
-http://www.ti.com/tool/TIDA-050023 seem ok for the power level but the Vin range is too little (42 to 57V).
For the DC/DC portion the http://www.ti.com/tool/PMP7279 could be an option.
As starting point I looked at the below but I was not able to find something that closely match the specs:
http://www.ti.com/reference-designs/index.html#search?intype=DC&keyword=poe%20pd
Thanks in advance,
A.