This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] UCC21710QDWEVM-025: differences vs UCC21750QDWEVM-025

Expert 6460 points
Part Number: UCC21710QDWEVM-025
Other Parts Discussed in Thread: UCC21750QDWEVM-025, UCC21710, UCC21750, UCC21710-Q1

Team,

1. What is the difference between UCC21750QDWEVM-025 and UCC21710QDWEVM-025, besides different driver?

2. Can UCC21750QDWEVM-025 be used to evaluate also UCC21710? 

  • Hi Bart,

    1. The boards two EVMs are the same aside from the driver and a few different components populated based on the type of short circuit detection, where UCC21710-Q1 uses OC and UCC21750 uses DESAT. The differences are noted in Section 3.1 (specifically pg. 22) of the User's Guide.

    2. Yes, the EVM boards are the same with just the differences I mentioned above. Just the components mentioned in the User's Guide should be changed based on which device you are evaluating. 

    Regards,

    Audrey