Hi,
I am trying to use a constant current LED driver.
My input is Vin = 3.3V and PWM = 1khz (duty cycle is 0 to 50%). I would like to control one LED (Vf= 2.95) with 1A.
So I set up based on the datasheet, which I follow the typical circuit (R1=200m ohm).
1. First, I wonder LM3410 is a good option for me. I need a constant-current circuit (which can be 0.5A-1A) and PWM controls (1K and duty 0-30%).
2. I quickly tested it, but the output is not the same pulse as PWM. My duty cycle keeps changes, but the output is a constant value (approx 3V).
My test condition is similar to Figure 27 (8.2.8 on page 27 datasheet). I also used the same value for C, L and R1.
Can I have any simulation for this circuit (e..g, Tina)?
3. If this is not relevant, would you recommend any circuit that fits my requirement?
Thanks