Dear Audrey,
I have tested the IC - ISO5452 along with IGBT - SKM150GB12T4.
Following is the details as mentioned below:-
Vp = 15V.
Vn = -6.8V.
Rg = 1.2 ohm.
I have shown the image of Vge below:-
There is slight dip in gate emitter voltage at turn on and turn off which can be seen by red circles.
Kindly enlighten me on the same.
Thanks & Regards,
Vedang.