Can you please provide the timing details of Power Up and Down sequencing for TPS53622, its NOT mentioned in the datasheet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you please provide the timing details of Power Up and Down sequencing for TPS53622, its NOT mentioned in the datasheet
Hi Abhishek,
There is no special timing requirement of TPS53622.
Please check the recommended sequence in datasheet section 7.
The recommended power-up sequence is:
1. 3.3 V
2. 5 V
3. PS_EN
4. 12 V
5. VR_EN
The recommended power-down sequence is:
1. VR_EN
2. 12 V
3. PS_EN
4. 5 V
5. 3.3 V
Thanks
Chasel