This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650243-Q1: TPS650243-Q1 DCDC3 Iout current.

Part Number: TPS650243-Q1
Other Parts Discussed in Thread: TPS65023-Q1

Dear TI Team.

The load current of the TPS650243-Q1 is indicated as 0.8A up to 1A.

We are going to use 1V 1A.

Is support available?

Thanks.

  • According to the "Voltage Options" table on page 3 of the TPS65024x-Q1 datasheet, the TPS650243-Q1 can only supply up to 0.8A on DCDC3.

    Can you use TPS65023-Q1, which has same number of DCDC rails (DCDC1 up to 1.7A, DCDC2 up to 1.2A, DCDC3 up to 1.0A)?