Customer question:
I have a question regarding the connection for the microphone as described on the TPS65950 Data Manual. On page 90, it shows the microphone connected to MICBIAS1/2.out, MIC.SUB.P/Mic.Main.P, MIC.SUB.M/MIC.MAIN.M
Does it mean for RSM connected to both pins MICBIAS1/MICBIAS2.out, CSM.P to both MIC.SUB.P and MIC.MAIN.P, CSM.M to both MIC.SUB.M / MIC.MAIN.M?
Or Connect to only RSM to MICBIAS1.out, CSM.P to MIC.MAIN.P, CSM.M to MIC.MAIN.M? Or eitherConnect to only RSM to MICBIAS2.out, CSM.P to MIC.SUB.P, CSM.M to MIC.SUB.M?
Clarification:
To avoid similar diagrams all information was combined in one block diagram. So, consider this as two diagrams, one for main mic and other for sub mic.
Maybe it would be clearer if Rsm was written as Rsm/mm – meaning for sub-mic and main mic.