This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: output abnormal with load connected

Part Number: BQ77915


Dear,

our customer designed with BQ77915, 4 cell, schematic as follows, please help to review if anythig wrong here:

now we have two problems need help to solve:

1. 4 cell with 3.7V each, total is about 15V, but the output is about 10V without load connect,

2. output drop to about 0.8V if load connected

please help to advise, thanks.

  • Hi Laisan,

    I have reviewed your schematic and have some suggestions:

    1. Since you are not using external cell balacing FETs, the Rin values should be 33 Ohm, not 1k.
    2. CCFG should be pulled high for the 4S configuration, it seems that you have it connected to AVDD and ground. Double check the value on this pin.
    3. R47 needs to be removed. VC5 should not be connected to VC3 for this configuration.
    4. Could you explain why you have added extra caps and resistors on the SRP and SRN pins? I do not believe they are needed.
    5. The CBI pin needs a 10k Ohm pull down resistor.
    6. Rts_pu (R50 in your schematic) should be 10k, not 100k.

  • Dear,

    customer check item 6 and changed the R50 to 10K, and it works.

    please help to explain why?

    and customer will modify the rest of your advice and to check again,

    thanks.

    b/r

    vincent

  • Hi Laisan,

    I'm glad I could help fix your problem!

    The Rts_pu is a pull up resistor that is used to determine the temperature protection threshold. This behavior is described in section 10.1.1.5 of the datasheet. Changing this resistor value will impact other fault functions such as OTD, UTC, and UTD. I cannot say for sure what happened, but it is possible the device was in some sort of false fault condition.