This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072T: No output voltage if no battery - empty battery not charging

Part Number: BQ24072T

Hi,

I have a questions about the BQ24072T :

  1. I don't have output = Vbat + 225mV as datasheet say.
    1. Actually, with a Vout = Vbat

  2. If I only put the Vin, (no battery) Vout is approx 600mV, If I put a battery and remove the battery, Vout is ok (about 4.1V)
  3. If my battery are empty, BQ does'nt charge them (Vbat of 600mV).

My design :

Vbob = 5V

Vbat is a 3.7V li ion battery

Vreg = the output

I try with EN2 conneced to Vbob : same result