Other Parts Discussed in Thread: DCPA10505
Hi Team,
I would like to know about the Soft Start definition in the datasheet.
(1) “a delay of typically 10 ms before the output voltage begins to rise”
Is this an understanding of the pink part of the figure?
(2) What is the definition of “the soft start time is typically 5 ms”?
Is it ok to understand that the rise time of the output voltage (time to reach 10% ⇒ 90%) is 5ms in typ value?
Please illustrate if possible.
(3) What are the numbers (1) and (2) above for DCP010505DBP?
Is 0ms for (1) (no delay ≒ no intentional delay)?
Best Regards,
Kenji