On the enable pin of the LDO, is it pulled in either direction internally? What is the ramification of leaving it floating?
Looking at the block diagram in the datasheet, it doesn't look like EN is pulled internally.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
On the enable pin of the LDO, is it pulled in either direction internally? What is the ramification of leaving it floating?
Looking at the block diagram in the datasheet, it doesn't look like EN is pulled internally.
Hi Mitchell,
You may consider this enable pin as a logical signal that requires a either high "1" or low "0". Typically this pin is directly controlled with digital output and itshould not be left floating. There is no internal pull-up or pull-down for this device.
Regards,
Jason Song