This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG3410EVM-018: DC Bus input

Part Number: LMG3410EVM-018


Hi Team,

My Customer is asking if he can input 12-48V on the DC Bus in dc/dc converter power stage of LMG341xEVM-018?

Input voltage : 12~ 48V ( HighVoltageBus)

The plan is that use this EVM board in 12-48V Bidirectional DC/DC Converter

Looking forward to your inputs.

Regards,


-Renan

  • Hello Renan,

    The LMG3410 EVM is for 600V rated GaN FETs. So there is definitely no problem if you want to have 12-48 V on the DC bus. However, it is doubtful if this is a good solution for this level of voltage since using 600V FETs here can be very overkill.

    Thanks and regards,

    LIxing