This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548A20: Schematic Review for 12V to 3.3V 10A

Part Number: TPS548A20

Hi TI expert,

Could you help to review the schematic with TPS548A20? Do we need to consider to add heatsink since we need to support 70°C?

Vin: 12V (11V~12.9V)

Vout: 3.3V

Iout: 10A max (5A for the thermal and power loss consideration)

Operational Ambient: -10°C to 70°C

PCB layers: 10 layers. 

Some questions:

1. Do we need to consider to add heatsink since we need to support 70°C? The webench simulation result seems too good on efficiency, comparing a test result with 12V to 1V 15A 500Khz. 

2. Do we need to do bode plot test for such DCAP3 control? Will our design be stable? Per the datasheet, the LC pole and a zero are mentioned. But no much idea how to calculate the phase margin and cross-over frequency with the selected components.

 Thanks,

Dora