Hi TIs
I have two designs which need to integrate Type-C/PD power function.
One is 5/9/15/20V with MAX 3A power,
The other is 5/9/15/20V with MAX 5A power,
Could you please help to advice a power chip for me?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TIs
I have two designs which need to integrate Type-C/PD power function.
One is 5/9/15/20V with MAX 3A power,
The other is 5/9/15/20V with MAX 5A power,
Could you please help to advice a power chip for me?
Thanks
Hi Cun,
The TPS65987D would be a good fit for your application. You can refer to TIDA-050012 which is a TI-Design that I think can meet your needs.
Thank you,
Eric
Hi Eric
Thanks for your reply.
actually, I already have the type C PD controller, what I need is just a DCDC buck part which can output max 5A from 5V to 20V.
Could you please help to check if TI has those DCDC?
Roy
Hi Roy,
Perhaps you may be interested in using the LMZM33606 device. This 36V/6A DC-DC buck power module provides high efficiency with minimal external BOM (4 components) for a complete DC-DC solution in a compact 16mm x 10mm QFN package.
Regards,
Jimmy