This is with reference to evaluation board of LM5160A (http://www.ti.com/lit/ug/snvu408a/snvu408a.pdf).
Configuration which we are referring to is as below:
As per the above configuration, below are L_MIN Calculations, that is coming around 94uH.
Same 94uH is the calculated value from excel tool provided by TI (LM5160FBKQuickStartCalculator - FinalVersion.xls) and it is attached for reference.
Can you please help us to know the reason why a lesser value of primary inductance of 60uH is chosen instead of higher value than calculated value L_MIN of 94uH in evaluation board.
Thanks,
Dhoresh.1524.LM5160FBKQuickStartCalculator - FinalVersion.xls