This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65197: Can it support 8V VGH?

Part Number: TPS65197
Other Parts Discussed in Thread: TPS65190

Hi team,

My customer is looking for a level shifter with below specs.

  1. VGH 8V~12V
  2. VGL -8V
  3. 1.8V input signal
  4. >=6 channel

TPS65197 meets the 2nd~4th requirement, but seems doesn't meet 1st requirement. VGH range should be 16.5 V to 45 V as shown in datasheet.

Could you double check whether 65197 support 8V VGH?

If not support, can you recommend a suitable device?

Thanks,

Miranda