The TPS2540 datasheet shows a "Host Sense" block in the diagram on page 9, but doesn't describe its function. If the TPS2540 detects the DM_OUT and DP_OUT pins are in a device mode state, will it simply turn on the data switches from in to out?
If not, is there another way to get the TPS2540 to pass through the D+ and D- signals, but not pass power from the OUT pin? Or is there another product that behaves as a USB charge port power switch controller for a OTG device in host mode, but a signal pass-through when in device mode?