I use TL494 to design my circuit,I set the frequecny is 100kHz,CT is 4.7nF, RT is 2K variable resistance,
when I was test circuit,I find the duty isn't working in maximum,it was attenuation to 87%.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use TL494 to design my circuit,I set the frequecny is 100kHz,CT is 4.7nF, RT is 2K variable resistance,
when I was test circuit,I find the duty isn't working in maximum,it was attenuation to 87%.
Hi Wu Chen,
What is the voltage on the DTC pin ? The voltage on the DTC sets the dead-time of the PWM signal, see section 9.3.3 on page 11 of the datasheet for the description of operation.
To maximise the duty cycle the voltage on the DTC pin should be 0V.
Regards
Peter
The DTC voltage is 0V , and FB voltage is 0V ,too.
which is attenuation of maximum duty?
Hi Wu Chen,
I hope you have made some progress since Colin's resply. Since there has been no activity on this post for 5 days I will close the post.
Please open a new post if you have more questions.
Regards
Peter
hi,wu
I had the same problem,then i change CT LARGER.and reduce the frequency. the duty is 91%.
now i try to make the DTC VOLTAGE TO -0.3V.
BUT I am still finding the way to make the DTC VOLTAGE TO -0.3V
DO you ALL have some way to achieve this?
Thanks a lot
JI YUE
Hello Wu, Hello Ji
I don't think that pulling DTC negative is a good idea - it may work in the lab but there is a danger that the negative voltage could forward bias some internal junctions in the IC and cause a malfunction. DTC should be tied to 0V to minimise the dead time.
I don't see any way to increase the duty cycle beyond the device specification by making changes to RT or CT - there may be some small effect by reducing CT and increasing RT but it would be small.
One thing you should experiment with is to directly control the voltage on the FEEDBACK pin to greater than 3.5V - be careful to keep the current into the pin to less than 3mA (the recommended operating maximum). If this works you may be able to add an external pull up resistor from FEEDBACK to VREF or to VCC to increase the effective operating range of the IC error amplifiers.
Regards
Colin