This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2511: Issue when charging IPhone 6s

Part Number: TPS2511

Hi 

We see an issue that when charging iphone 6S, the iphone 6S touch response will delay.  Would you help review if below DP and DM behavior are correct ? 

Below are the waveform (Purple line is DM waveform, the Blue line is DP waveform)

1.  Waveform before connected to iphone 6S (DP is 2.84V、DM is 2.17V)

2. at the moment iphone connected, see DP and DM drop as below wave form. 

Then DP DM become this waveform 

finally it will settle at below waveform (within 20 sec after the iphone are plugged)