The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Isolated DCDC converter/Module

Other Parts Discussed in Thread: UCC12050, LM25180, TPS55010, UCC2805, LM5160A, TIDA-00349, TPS60402

Hello,

I need an isolated power solution that can take 5Vin, 5 or 3.3Vout, and 10mA out.

Would Flyback be the best solution here because of the need for isolation? Could you recommend best solution/direct me to the best family of devices?

Thanks,

Adam

  • Adam

    Our first recommendation is UCC12050, which is an isolated DC/DC module that will meet all of your requirements.

    If you would like to design your own power stage then a flyback controlled by either LM25180 (integrated FET) or UCC2805 (external FET) is recommended.  Alternatively a fly-buck may work well here, with TPS55010 (integrated FET) or LM5160A (external FET) recommended.  More information on flybuck is available at www.ti.com/flybuck

    Eric

  • Hello Eric,

    Thank you for your response. Looking at your recommendation, I don't think it will work because the load is only 6mA and at that load the efficiency is only 15%. Is there anything similar that has more efficiency at light load?

    Best,

    Adam

  • Adam

    If UCC12050 does not meet your requirement then I recommend one of the controllers where you can build your own power stage. These devices can be used in a power supply that is optimized for your design requirements. 

    TIDA-00349 is a reference design that is very close to your requirements that I recommend reviewing to see if it meets your needs.  It has much higher efficiency in the range you are concerned about.  This design uses TPS60402.

    Eric