Other Parts Discussed in Thread: TPS65261
Hi team.
Customers will use TPS65261 under the following conditions:
PVINx = 5V
Vout1 = 1.1V , Iout1 = 0.28A
Vout2 = 1.5V , Iout2 = 0.52A
Vout3 = 1.0V , Iout3 = 1.25A
The customer wants to control the sequence of this IC with the following configuration
figure1
But V7V was not output in this configuration.
If the connection was changed as follows, it worked as expected.
figure2
I want to know why V7V is not output when configuration of figure1.
Vest regards.