This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54627: Output voltage much lower than expected

Part Number: TPS54627

Hello,

We are using the TPS54627 with an input voltage of 9.3V; however, we see an output voltage of 0.509V.

Referencing the data sheet, we are using:

R1: 30kOhm

R2: 22.1kOhm

R3: 10kOhm

C1,C2: 10uF

C3: 0.1uF

C4: 10pF

C5: 1uF

C6: 8200pF

C7: 0.1uF

C8,C9: 22uF

L1: 3.3uF

Interestingly enough, the output voltage varies with our input voltage, peaking at 0.736V out with 13.1V in. The same phenomenon happens on two chips we tried. Any ideas? Leads?