Other Parts Discussed in Thread: PMP20588
I have copied the PMP20058 POE reference design to my circuit board with all the same parts including the Coilcraft transformer. My Vin is 12V and I expect 54V output. My design does not work, there is no output. Can you provide some troubleshooting tips based on the PMP20058 schematic where I can start looking to find the issue? Are there changes I can make to the circuit to force it to start up so I can then continue to trouble shoot? Are there test results and waveforms available for the PMP20058 circuit that I can compare with my circuit.