Hi,
It indicates the Max Pulse Drain Current is 85A in the datasheet, which is under condition that the pulse duration <=300us and the duty cycle <= 2%.
- In application, If the current exceed 85A, but the duration is much lower, single pulse less than 10us, is there any problem?
- Is this IC is wire bonding or Die connects to the leads directly?
Thanks.