This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD17527Q5A: Current Rating

Part Number: CSD17527Q5A

Hi, 

It indicates the Max Pulse Drain Current is 85A in the datasheet, which is under condition that the pulse duration <=300us and the duty cycle <= 2%.  

  1. In application, If the current exceed 85A, but the duration is much lower,  single pulse less than 10us, is there any problem?
  2. Is this IC is wire bonding or Die connects to the leads directly?

Thanks.