Other Parts Discussed in Thread: LM46001, LM46000, LM5117, LM5116, LM5145
Is there a similar Part with almost the same parameters (Frequency, RDSon..) and package like LM46002 but with adjustable current limit?
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Michael,
Most of our part has a fixed current limit such as LM46000, LM46001. They are pin to pin compatible with LM46002 but at lower current.
Is there a specific current that you are looking for?
Otherwise there is a controller who is most likely has an adjustable current limit. The controller has external FETs instead of internal one such as LM46002
Thanks
-Arief
Hello Arief,
No specific current value but i want to adjust it in the application as necessary.
which controller do you mean exactly with the adjustable current limit?
Best regards
Michael
Hi Michael,
Maybe something like this part? LM5116 or LM5117
http://www.ti.com/product/LM5116
Or this one which is relatively newer part LM5145
http://www.ti.com/lit/ds/symlink/lm5145.pdf
Thanks
-Arief