Other Parts Discussed in Thread: BQ25125
Hi Team,
We have selected BQ24092 IC for Single cell Li-ion battery charger for Outdoor asset tracking applications.
Charging input voltage is from the USB 5.0.
device max current is 200mA at data transmission.
Device voltage should be 3.8V constant
Battery Spec:
Capacity:3400mAh (Min 3250mAh)
Nominal Voltage: 3.7V
Charging voltage:4.2V
1. Using BQ24092 Charger how to limit the output voltage to 3.8V.
2. How much is the time taken to charge the battery using USB?
3.Any probelm is there, If I connect the load in parallel to the battery when the battery is charging through USB?
Please support on the above questions.