Other Parts Discussed in Thread: INA169,
Hi team,
I would like to ask if the LD Current is to be controlled within +/- 6% (including Ripple noise), if it is applied with LM3409HV.
1.) How can we modify the surrounding schematic as below link to achieve it?
2.) If the INA169 current sensor is connected in series with the LED driver Output, then it is detected by the MCU ADC Pin, and then used to dynamically adjust the LM3409HV IADJ to correct the current, is it feasible, or is there any other suggested way? Thanks.
https://txn.box.com/s/qtqupdiwpj2mrsbk8nyp5yfm2ba0d68g