Hi
It's mentioned at datasheet about "PWR ON enable" condition as below,
1) None of the device POWER ON disable conditions are met.
2) PWRON signal low level
Or PWRHOLD signal high level.
But PWRON signal must be low when PWRHOLD signal rising up.
(This was explained at previous post.)
https://e2e.ti.com/support/power-management/f/196/t/862132?tisearch=e2e-sitesearch&keymatch=TPS65911
So that, 2) is should be, PWRON signal should be low level "AND" PWRHOLD signal high level".
Q1:Is this correct? (Not "Or" condition)
+Looking at the logic circuit diagram below, it looks like “OR”.
On the other hand, Switching-ON and OFF sequence is started by PWRHOLD. (Fig 5-1)
Q2: So, if we want to start the Switching ON in this case ,can the customer control by PWRON signal after the above PWR ON sequence such as from state of PWRON =high and PWRHOLD = high?
Best Regards,
Koji Hamamoto