Other Parts Discussed in Thread: TPS65982
I have the following circuit http://www.ti.com/lit/df/tidrgw6/tidrgw6.pdf, where External Power is 5 - 20V and HV_Source gives 12V. HV_Source is connected to a input pin on TPS65982. The problem is that i need to configure the TPS65982 pin as output and i need to know , what will happen if External Power will be 0V (unconnected) and HV_Source is 5V. Is there risk of destroying the TPS54335 chip and if so , what should i do to safely test this? Unsolder L4? or just pull down the EN pin? Also what would happen if External Power would be like 5V input and HV_Source would be 5V input? Any help is appreciated.